It seems that depending on which family of MCU I chose, I am limited as to how many VCPs I can have.
For instance, I _think_ the LPC11U68 is limited on endpoints so just one VCP is possible. AN12458 states the LPC54018 can have two VCPs on the high speed and another two VCPs on the full speed - which sounds confusing - shouldn't ten physical endpoints support at least three VPCs? Maybe it's how they are allocated...
So, which LPC's would give me the most? Is there an easy way to determine how many VCPs I can run on a particular device?
The application is a single MCU that has several different UARTs with various proprietary protocols, so I'm trying to get the chip count down as low as possible. There's not a lot of processing, so an M0 core is adequate. I just want a single device that appears as multiple comm ports.
Hello Chris
To select the LPC MCU I recommend you to follow this mini-guide that I´ve made.
Each VCP will require 3 endpoints.
Endpoints requirements for VCPs
Take into account that the packet size of each endpoint is stored into an endpoint buffer RAM.
You should take into account the following considerations to calculate how many
VCP´s will support an MCU.
Now take a look at these examples
This is the table of endpoints for LCP1311, which supports only one VCP
There are only 6 endpoints of interrupt or bulk type.
For another VCP the LPC1311 must have another EP with in direction. In this case
endpoint buffer RAM was enough to cover EP buffer size.
The LPC17 Supports 32 physical (16 logical) endpoints and has a 4 kB endpoint buffer RAM.
For the LPC5400 case:
Its USB0 device controller supports 10 physical (5 logical) endpoints including two control endpoints.
Its USB1 device controller with the specification for high speed supports 8 physical (16 logical) endpoints with up to 8 kB endpoint buffer RAM. Control, Bulk, Interrupt and Isochronous endpoints are supported.
I hope this information helps you, best regards.
Have a great day,
Diego
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------