I want to know the different of performance bettween SAI1 and SAI3.
As i know the SAI1 from M4 and SAI3 from A53.So can I use the SAI3 to send the music to the audio card? Thanks a lot!
或者我这样问 SAI3 是否支持DSD512 谢谢
Hello,
For which i.MX are you talking for?
Best regards,
Diego.
Hi ,
I want to know that about IMX8M mini.
1.I see the SAI1(3.3V ) also used for boot CFG .If i change the power of SAI1(3.3V ) to SAI1(1.8V) ,also to every part about SAI1.
Does the boot CFG work normal ? As i need use the SAI1 works at the level of 1.8V ranther than 3.3V.
thanks a lot !
According to the i.MX8MM datasheet. There is no problem if you use 1.8 to supply the SAI1. It supports voltages from 0V to 3.8V
Best regards,
Diego.