In our circuit diagram, PIN0_2 and PIN0_3 are used as serial ports. PIN0_2 and PIN0_3 are configured as USART3.But can not output messages.What should I pay attention to when configuring as usart3.Thanks.
In our circuit diagram, PIN0_2 and PIN0_3 are used as serial ports. PIN0_2 and PIN0_3 are configured as USART3.But can not output messages.What should I pay attention to when configuring as usart3.Thanks.
Hi Omar:
Thanks!
B/R
Aifei Zhang
发件人: nxf54944
发送时间: 2019年12月6日 5:09
收件人: Aifei Zhang
主题: Re: - Re: LPC54016JET100 Usart config problem
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: LPC54016JET100 Usart config problem
reply from Omar Anguiano <https://community.nxp.com/people/nxf54944?et=watches.email.thread> in MCUXpresso Software and Tools - View the full discussion <https://community.nxp.com/message/1242113?commentID=1242113&et=watches.email.thread#comment-1242113>
Hello, 爱飞 张
In this image, you can find the initial configuration of the usart according to the user manual. Please make sure that the pin mux is the correct one, refer to table 239 of the same user manual. LPC540XX Family of Microcontrollers (MCUs) | NXP
I suggest referring the SDK examples to config your usart along with examples to transmit messages. https://mcuxpresso.nxp.com/en/welcome
Let me know if this is helpful.
Best regards,
Omar