According to the UM,This bit can be written only in Freeze mode。But I'm already in freeze mode,It's no use writing 1,The register value was found to be 0 when debugging with lauterbach,Before that,FRZ bir is 1, FRZACK bit is 1, and HALT bit is 0。Even if I don't set HALT to 0,When I've set up the MAXMB bit, HALT automatically goes to 0。
Could you tell me the reason why I failed to write IRMQ?
Hi,
the code is wrong, clearing HALT bit should be last instruction during initialization.
Anyway you should be able to set IMRQ using debugger in debug mode or not?
BR, Petr