LS2088 reassembly performance using AIOP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS2088 reassembly performance using AIOP

556 Views
wille_kuutti
Contributor I

What kind of real reassembly performance you have archieved with LS2088 SoC using AIOP? Is 10Gb/s realistic expectation when reassembling jumbo frames (9000 bytes) from 1500 byte fragments?

Br,

Wille

Labels (1)
Tags (1)
0 Kudos
1 Reply

474 Views
bpe
NXP Employee
NXP Employee

Performance is a delicate matter which requires individual discussion
and comments for each use case to ensure the benchmarking test conditions and
numbers we provide are properly understood. For this reason, no benchmarking
information can be published through this Community is addition to
what is available on the official Web resources, namely, up to 20 Gbps packet processing by AIOP.

Customers wishing to receive more specific performance estimations and/or benchmarks are
advised to discuss it with distributors.

Regards,

Platon

0 Kudos