i.mx8 USB DRD as USB3.0 SS Host

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx8 USB DRD as USB3.0 SS Host

685 Views
ralf_oberlaende
Contributor I

Dear NXP support,

I have an issue regarding USB connectivity for the i.mx8 Soc:

The hardware has 2 usb components inside: one host and the other one is usb dual role capable.

I have the dual role instance configured for host mode, but I can't enumerate devices in superspeed - highspeed works well.

The device (in my case a hub) is connected using a special cable with a micro-a-plug.

I'm using the Nitrogen8M hardware with ubuntu linux.

How is the procedure to get USB SS devices working on that USB instance?

0 Kudos
0 Replies