Hello NXP,
Does the lsdk_linux_arm64_tiny.itb is different from LS1088 and LS2088. If different where can I get LS2088 arm64 tiny lib file.
regards,
ranga
The lsdk_linux_arm64_tiny.itb includes kernel, .dtb file and root file system for all arm64. it includes the LS1088a and the LS2088a.
This .itb file is built using .its file. See the linux_arm64_LS.its using the following path:
/LSDK_1909/flexbuild_lsdk1909/configs/linux
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------