when i use gplay-1.0 to play a music file, then i click into back camera,gstreamer has a warn: alsa gstalsasink.c:989:xrun_recovery:<alsasink1> xrun recovery -32: Broken pipe
why have this error, What is the situation this error produce? and music can not playing.
i use imx6q board, bsp is fsl-release-bsp-L4.1.15_2.1.0.
Hi Max
one can test on i.MX6 Sabre SD reference board with Demo Images from link
i.MX Software and Development Tools | NXP
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------