AnsweredAssumed Answered

CLRC663 - GPIO Behavior

Question asked by Jonathan Frech on Nov 27, 2019
Latest reply on Dec 6, 2019 by Kan_Li

Hi,

 

I'm using the CLRC663 to display status leds on a application. When entering low power mode, i shut down the CLRC663 to save power by the hard power down (setting PDOWN high)

 

Now, when exiting the PDOWN state, i see all leds flash visually, which is an issue to the device, since it looks very weird.

 

I took a measurement with a oscilloscope and below you can see what i see (only the first sequence is relevant). The MCU boots and enables power to the device and immediatly sets PDOWN Pin high (CLRC663 shutdown). After intializing alot of peripherals, the MCU wants to initialize the CLRC663. For this PDOWN is set low.  100us later, OUT 1 Pin gets high for around 5-6ms before comming low again. As you can see on the scope, the OUT1 pin goes only to about 2V's, instead of 3.3V (PSU Voltage). When switching the IO's regulary in Software, the level is correct at 3.3V

I only put PDOWN low and then immediatly send command to put the device in sleep (software). I do not make any other changes to the CLRC663 at that point


For usage of IO's i disabled the Boundary Scan interface in eeprom.

 

Any Idea why this happens?

 

Scope  Screenshot

Outcomes