Mo Abbasi

BOARD_XTAL0_CLK_HZ is always 12MHz with Clock Config Tool

Discussion created by Mo Abbasi on Nov 27, 2019
Latest reply on Dec 3, 2019 by Alexis Andalon

I'm using web clock config tool to setup the clock and generate clock_config.c and clock_config.h files, and then I export the two files into my project. Sometimes I select a board e.g. "LPCXpresso54618" and sometimes I select a processor e.g. "LPC54605J512" to start with and then I make my desire changes. 

I have a 24MHz xtal on my board, so I change the "clock input" to 24MHz and change the "system oscillator freq range selection" to High Frequency. 

As far as I can see, everything works fine, but I have noticed that BOARD_XTAL0_CLK_HZ in clock_config.h file is always set to 12MHz. Maybe it is not used any where. 

 

define BOARD_XTAL0_CLK_HZ                         12000000U  /*!< Board xtal0 frequency in Hz

 

clock config tool

xtal0 xtal in mcuxpresso configtools

 

BR

Mo

Outcomes