Problem with include files

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with include files

712 Views
juliancox
Contributor V

I have a CW11 project for a MC9S08QE processor using ProcessorExpert.

The significant components are SPI master (SM1) and a Free counter (FC1).

The projet comprises four files, main.c, main.h, events.c and events.h. The only include statements are 

#include "main.h" in main.c and 

#include "events.h" in events.c

When I declare a variable in one .h file and declare it as external in the other I get the error:

ERROR L1818: Symbol 24 - HexTemp duplicated in SM1_c.obj and Events_c.obj.

I get the same error message for up to 10 variables and sometimes the first reference is CPU.c.obj.

 I tried re-naming the variable to no avail and I also tried deleting the offending .obj files.

I get the same problem when I cut from main .h file and paste it into events.h.

My only solution is to cut the offending variable from events.h and paste it into events.c and then I get no errors.

I re-created a new project with the same components and I got the same problem.

Labels (1)
Tags (1)
0 Kudos
1 Reply

594 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  Julian Cox,

Could you please send your project or a simple project that can reproduce the issue,

I will check it  on my side.

BR

Alice

0 Kudos