S32DS S32k146SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS S32k146SDK

671 Views
oceansea
Contributor III

hi,

i use the S32K146 MCU  ,and i do this 

New->S32DS Project From Example,is OK,and i look the sdk

pastedImage_1.png

It show this example use the  S32K146_SDK RTM3.0.0

So i  make sure my IDE installed S32K146_SDK RTM3.0.0 .

But when i do this ,   New->S32DS Application Project ,

pastedImage_2.png

pastedImage_3.png

I can't use S32K146_SDK RTM3.0.0  ,and when i go on ,finish creat project.

pastedImage_4.png

pastedImage_5.png

it may be said the S32K146_SDK RTM3.0.0 is damaged.

Then  i  found the different from the Examp prj  and my prj ,

the Example use ARM Bare-Metal 32-bit Target Binary Toolchain;

and my prj use Stander S32DS toolchain for ARM.

If has any different about these toolchain?

Because i wat use S32K146_LQFP64  so i have to use S32K146_SDK RTM3.0.0

Labels (2)
Tags (1)
0 Kudos
0 Replies