I have a box of these boards in my stock and cannot figure out if I need them or not, seriously can't find anything on them through my normal database. I know it's a long shot but was wondering if anyone here can help me identify what this board goes to and/or is used for it runs on a Coldfire MCF5213 connects via USB by FTDI. I know this is not a normal question here but it seems like this chip is pretty specialized so thought I may get lucky posting a few photos of the board on here seeing if someone knows theboard or could point me in the right direction on where I should start searching. Thanks in advance for any information.
It would help to work out what it is if you could post the part numbers of the other large chips on the board.
I suspect it is some sort of function add-on board for a printer.
Tom
Hi,
It is not a MCF5213 evaluation board for sure.
There with HP logo, could be circuit board used for HP products.
Have a great day,
Mike
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------