Hello !
Can pin be inverted first and after that contribute to GINTx group ?
For example Rising edge will be inverted to falling edge and after that is detected by GINTx ?
And wakeup capabilities from POWER DOWN mode is not degrade.
or pins connected to GINTx directly and no inversion is possible :
"
The pins can be configured as GPIO pins through IOCON, but they don’t have to be. The
GINT block reads the input from the pin bypassing IOCON multiplexing. Make sure that no
analog function is selected on pins that are input to the group interrupts. Selecting an
analog function in IOCON disables the digital pad and the digital signal is tied to 0.
"
Regards,
Eugene
Hello Eugene,
Let me know if I understand correctly:
You want to invert the polarity after detecting one of the edges rising. If that is the case it shouldn't be a problem for the wake up from POWER DOWN.
Let me know if this helps you.
Best Regards,
Alexis Andalon