About Boot Config of evaluation board (MCIMX7D-SABRE)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About Boot Config of evaluation board (MCIMX7D-SABRE)

Jump to solution
537 Views
goto11
Contributor III

Hello,Community


LCD1_DATA [0:23] and 10kΩ pull-down resistor are connected.

Table 96 of the data sheet describes "100K Pull Down" during State during reset.

If i.MX has a pull-down resistor, can I remove the external pull-down resistor?

best regards

Goto

Labels (1)
0 Kudos
1 Solution
460 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  Although table in i.MX7 Datasheet(s), named "Fuses and associated pins used for boot"

shows default boot pins states - the following is provided in Table 3 (LCD recommendations

for developer's boot modes) of “Hardware Development Guide for i.MX7Dual and 7Solo

Applications Processors”:

 

  "The BOOT_CFG signals are required for proper functionality and operation and should not be left floating".

 

  That is - external resistors should be applied.

 

 http://www.nxp.com/assets/documents/data/en/user-guides/IMX7DSHDG.pdf

 

 

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

View solution in original post

0 Kudos
1 Reply
461 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  Although table in i.MX7 Datasheet(s), named "Fuses and associated pins used for boot"

shows default boot pins states - the following is provided in Table 3 (LCD recommendations

for developer's boot modes) of “Hardware Development Guide for i.MX7Dual and 7Solo

Applications Processors”:

 

  "The BOOT_CFG signals are required for proper functionality and operation and should not be left floating".

 

  That is - external resistors should be applied.

 

 http://www.nxp.com/assets/documents/data/en/user-guides/IMX7DSHDG.pdf

 

 

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos