Time resolution of a current-to-digital converter in NHS3152

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Time resolution of a current-to-digital converter in NHS3152

534 Views
younggeun
Contributor I

I want to read a real-time signal by NHS3152 NFC chip, through the current-to-digital converter.

What is the time resolution (from one data point to the next data point.. maybe the sampling rate?) of the chip?

I expect to measure body signals with a time resolution of sub-millisecond.

Young-Geun

0 Kudos
1 Reply

480 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Young-Geun,

I think you are referring to the sample rate/integration time, which is supported from 10ms to 400ms. Please refer to the following for more details.

pastedImage_1.png

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos