How to test USB2514i (hub) eye diagram in imx6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to test USB2514i (hub) eye diagram in imx6Q

566 Views
zohanlin
Contributor IV

Dear all,

I want to test the USB2514i eye diagram in imx6Q, and it is connected to USB HOST.

I use the command as below :

memtool -32 0x020c4080=0x3

memtool -32 0x02184340=0x2
memtool -32 0x02184384=0x1C040000

I can detect the signal between CPU and HUB, but I can't detect anything between HUB and miniPCIe.

Could anyone tell me how to solve the problem?

Thanks,

zohan

Labels (3)
0 Kudos
1 Reply

496 Views
igorpadykov
NXP Employee
NXP Employee

Hi zohan

from i.MX6Q usb side one can try to follow procedure described on

I.MX6 series USB Certification Guides 

for USB2514i eye diagram may be suggested to apply to vendor of that chip Home | Microchip Technology 

http://ww1.microchip.com/downloads/jp/DeviceDoc/jp567224.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos