Hi,
When I debug the SCH-27513 MPC5744 with S32DS POWER it has the errors:
how could I solve it?
Regards,
chinna
Hi,
From your screenshot it looks that you are using incorrect gdb executable. Please check your GDB settings:
Jiri
I am also having same configuration. Still, I am facing the same issure.
Hi,
make sure, that ${cross_prefix} contains correct value in project properties:
Or you can write it manually into debug configurations or manually browse the executable:
Also re-install may help to setup env variables correctly.
Jiri
Hi,
please check this thread:
https://community.nxp.com/message/1061805#comment-1117638
Which version of S32DS are you using?
If you are using v2.1 please check this:
https://community.nxp.com/docs/DOC-344945
hope it helps.
Regards,
Stan
S32DS_Power_Win32_v2017.R1_b171019