Board: MIMXRT1060-EVK
OS: Linux
SDK: SDK_2.6.2_EVK-MIMXRT1060.tar.gz
Sample binary flashed: hello_world (from demo_apps folder in SDK)
The board 1060 is not getting flashed with hello_world.bin, "FAIL.txt" file is getting generated. The "FAIL.txt" file says "The interface firmware FAILED to reset/halt the target MCU type : target"
The binary file flashing was tried with both QSPI Flash boot mode and Serial downloader mode.@
How can we resolve the issue? Is there any way to factory-reset the board?
Hi ,
Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
I'd like to get more information about the flashing failure, so I was wondering if you can introduce the steps of testing you did.
In further, I've attached the files which present how to program the QSPI in different IDEs and through the MCFtool, please refer to them for details.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------