I am working on USB 3.0 gadget on LS1046ARDB. I see LS1046ARD document "QorIQ LS1046A Product Brief"
The USB 3.0 module operates in following modes:
• Host Mode: SS/HS/FS/LS
• Device Mode: SS/HS/FS
• OTG: HS/FS/LS
Does the LS1046ARDB support Super Speed on Device Mode? Does it support UB3.0 (5Gbps) on Device mode ?
Thanks
Both answers - yes.
The LS1046A USB3.0 controller Device mode is supported by Linux kernel Gadget driver - please refer to the LSDK Documentation:
Submit Form
section "Device mode (Gadget driver)".