Good Morning,
Please see the attached document.
zip pass 777
Thanks,Regards,
Badri.
+918985740150.
From: nagajyothig@ngetpl.com
Sent: Wed, 08 Jul 2015 05:16:33 +0000
To: discussions-community-about@mail.freescale.jiveon.com
Subject: MPC8640D Failed to reset the target (core did not halt)
Hi all, we are working on a project CPCI Based SBC Board using MPC8640D processor. We are trying to get simple JTAG connection to the processor mpc8640d. We are using code warrior USB tab s/n 0839 0023. In code warrior, when I try to reset the MPC8640D core (via reset target on launch), it gives the following message:“CCSProtocolPlugin: Failed to reset the target (MPC8640d Core: Core did not halt).”
we are monitoring the jtag signals also , HREST and SRESET signals are not coming..by default these signals are in high state(+3.3v). Can you give me some guidance in interpreting this error ? Thanks and Regards, Jyothi
The "info_11_14.doc" provided in the ZIP contains virus.