I install Codewarrior v6.3,prompted bellows:
Codewarrior Development studio for Microcontrollers v6.3 is not compatible with windows XP 64-bit installation;
How can I solve this problem?
Hi,
CW6.3 can't support win7 64bit.
If you use HCS08 MCU, please use CW11 instead which is for 64 bit platform:
CodeWarrior® for Microcontrollers-Eclipse IDE 11.1 | NXP
Have a great day,
Jun Zhang
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------