AR0144 camera create video on i.MX8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AR0144 camera create video on i.MX8

837 Views
xu_ji1
Contributor V

Hi,

I used AR0144+max96705+max9286 on i.MX8 QM,I want to get AR0144 data then create video stream use VPU,

does VPU support the AR0144 pixel format output ?

How to make video about the AR0144 mono sensor?

Thanks

0 Kudos
3 Replies

711 Views
igorpadykov
NXP Employee
NXP Employee

Hi Xu

one can look at

AR0144 and ov9284 drivers for I.MX8QM/QXP. | NXP Community 
GitHub - sheeaza/vulkan-v4l2 at ar0144 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

711 Views
xu_ji1
Contributor V

hi,

I want to use this camera make avi or mp4 not photo use VPU encode,is there API in VPU for Y12 input format?

Thanks

0 Kudos

711 Views
xu_ji1
Contributor V

AR0144 output Y12 format data and give it to VPU encoder.is it support by VPU encoder?

0 Kudos