AnsweredAssumed Answered

Bluetooth: BD Address is AA:AA:AA:AA:AA:AA

Question asked by weibin chi on Nov 13, 2019
Latest reply on Nov 17, 2019 by igorpadykov

Hello

       I am using imx6dl processor interfaced with the wifi/bluetooth module ap6255.

       The bluez version is 5.51.

       Before turning on the bluez service,the BD Address is 6C:21:A2:58:E8:E3.

       I execute the command “/usr/libexec/bluetoothd -C & ”, start bluetooth.The phenomenon is as follows:

root@imx6qsabresd:/mnt/flash/user/yxapp# hciconfig -a
hci0: Type: BR/EDR Bus: UART
BD Address: AA:AA:AA:AA:AA:AA ACL MTU: 1021:8 SCO MTU: 64:1
UP RUNNING ISCAN
RX bytes:38753 acl:267 sco:0 events:1035 errors:0
TX bytes:33964 acl:282 sco:0 commands:610 errors:0
Features: 0xbf 0xfe 0xcf 0xfe 0xdb 0xff 0x7b 0x87
Packet type: DM1 DM3 DM5 DH1 DH3 DH5 HV1 HV2 HV3
Link policy: RSWITCH SNIFF
Link mode: SLAVE ACCEPT
Name: 'imx6-bt'
Class: 0x100100
Service Classes: Object Transfer
Device Class: Computer, Uncategorized
HCI Version: 4.1 (0x7) Revision: 0x0
LMP Version: 4.1 (0x7) Subversion: 0x6119
Manufacturer: Broadcom Corporation (15)

 

How is this solved?

 

Thank you!

       

Outcomes