Anoop R Nair

LPUART receive function not working (LPUART_DRV_ReceiveData) with SDK 3.0.0

Discussion created by Anoop R Nair on Nov 6, 2019
Latest reply on Nov 13, 2019 by Diana Batrlova

Hi,

Thanks Diana Batriova for the reply.

 

Feature:Porting of sdk 0.8.6 echo example(without processor expert) to

sdk 3.0.0(with processor expert) Serial communication with LPUART

Scenario: echo testing with LPUART

Given:start up code initialization done,

Given: clock configuration is done

Given: LPUART2 initialization done,

When:trying to transmit(using LPUART_DRV_SendData) it is able to

receive in terminal.

and trying to receive data(using LPUART_DRV_ReceiveData) from terminal

Then:device should receive.

Observation: Device is unable to receive data.

Indiviual sdk example are working fine.But when Iam trying to use

LPUART echo example code from sdk 0.8.6(without processor expert) to

sdk 3.0.0(with processor expert),receive(LPUART_DRV_ReceiveData)is not

working for me.

 

Outcomes