Hi all,
I have a question about usage of power MOSFET in i.MX6SLEVK.
I'm checking the schematic (iMX6SLEVK_DESIGNFILES/Schematics/spf-27452_b.pdf).
I can't understand that the usage of power MOSFET in P6 (Please see attache).
I understand that USB_VBUS doesn't have any power-up sequence.
Could you tell me why does it need ?
Furthermore, can user remove it ?
Ko-hey
Solved! Go to Solution.
The Q30 FET in the i.MX6SL EVK design is used as the workaround to the silicon erratum ERR006281 to isolate the USB_OTG1_VBUS rail from the USB OTG connector's VBUS contact until the VDDHIGH_IN voltage is applied. Better is to keep it in the custom design.
Best Regards,
Artur
The Q30 FET in the i.MX6SL EVK design is used as the workaround to the silicon erratum ERR006281 to isolate the USB_OTG1_VBUS rail from the USB OTG connector's VBUS contact until the VDDHIGH_IN voltage is applied. Better is to keep it in the custom design.
Best Regards,
Artur