AnsweredAssumed Answered

How to set IMX8MM colour space for G2D conversions

Question asked by brenhale on Oct 30, 2019
Latest reply on Dec 17, 2019 by Joan Xie

The IMX8MM reference manual section on the G2D specifies support for BT.601 and BT.709 YUV to RGB color conversions, including the formulas used. How are these set as they are not exposed in the G2D API?

 

  

14.2.2.4.8 YUV to RGB Conversion
YUV data can be converted into 8-bit per component RGB format at the output of the
cache only. Once converted, there is no way back to YUV format. GPU supports BT.601
and BT.709 YUV to RGB color conversion standards.

  

...

Outcomes