AnsweredAssumed Answered

How to extend a V4L2 control

Question asked by Michael Stahl on Oct 29, 2019
Latest reply on Nov 11, 2019 by Joan Xie

Hello,

I work with a i.MX6Q and connected an quad video encoder chip over CSI-0 interface. The encoder chip streams the data via BT656 and has a I2C control bus.

On software side I use the mxc_v4l2_capture.c drive and a modified ov5640.c driver.

In basic it works. I can display a stream via Gstreamer.

But I want to add a control for switching between the 4 input lines of my encoder chip.

 

My first thought was to add new control on base of V4L2_CID_USER_IMX_BASE.

So I call a IOCTL function with VIDIOC_S_CTRL and a parameter maybe V4L2_CID_USER_IMX_BASE.

But in that case I had to modify the mxc_v4l2_capture.c and my driver.

It's a way, but is it the right way? If I do that in that way, is there a possibility to control the capture input of my encoder chip by a standard application like v4l2-ctl?

 

Are ther other, better, ways to do that?

 

Thanks

Michael

Outcomes