Hello, All
Our custom board is designed the DDR parts with the mx6sabreauto RDK board.
It could get the RDK schematic from https://www.nxp.com/webapp/Download?colCode=SABRE_AI_DESIGNFILES_CPU2&appType=license .
The plan is as follow :
Our board is not ready and the first one will use 1GB - If it needs more, will use 2GB.
Use 1GB DDR - 256M x 16 x 2ea - Bus Width 32bits
Use 2GB DDR - 256M x 16 x 4ea - Bus Width 64bits (like RDK)
Each DDR parts are connected to imx6dl AP as follow: (the same schematic of MX6 SABREAUTO RDK)
U3 : CS0, SDCLK1, D0-D15
U5 : CS0, SDCLK1, D16-D31
U2 : CS0, SDCLK0, D32-D47
U4 : CS0, SDCLK0, D48-D61
I wonder that is it work to use only U3 and U5 ?
I checked about the DDR3 register programming from https://community.nxp.com/docs/DOC-105964.
There are to select the chip select and the bus-width in this excel file.
And https://www.nxp.com/docs/en/application-note/AN4397.pdf - the document doesn't comment anything about my case.
Could you help that it is possible only use U3, U5 or U2, U4 parts for 1GB ?
If it is possible, where should I modify in uboot/kernel ? I checked mx6dl.cfg and configuration excel files, but I was not found.
Regards,
Solved! Go to Solution.
Hello,
It is possible to use the following configurations:
U3 - for 16-bit data bus port;
U3,U5 - for 32-bit data port;
U3,U5,U2,U4 - for 64-bit data port.
Use Chapter 3 (Porting U-Boot) of i.MX_Porting_Guide.pdf in Linux documentation.
https://www.nxp.com/webapp/Download?colCode=imx-yocto-L4.14.98_2.0.0_ga
Have a great day,
Yuri
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
Hello,
It is possible to use the following configurations:
U3 - for 16-bit data bus port;
U3,U5 - for 32-bit data port;
U3,U5,U2,U4 - for 64-bit data port.
Use Chapter 3 (Porting U-Boot) of i.MX_Porting_Guide.pdf in Linux documentation.
https://www.nxp.com/webapp/Download?colCode=imx-yocto-L4.14.98_2.0.0_ga
Have a great day,
Yuri
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
Thanks for your reply.