i.MX6Q/D/DL/S SDIO bus speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q/D/DL/S SDIO bus speed

Jump to solution
888 Views
andychien
Contributor III

Dear Sir, 

Our customer used i.MX6Q/DL/S and confuse about SDIO bus speed.

Could you help check uSDHC (SDIO) support 208MHz on all port (1/2/3/4)

And How to setting 208MHz

Thanks, 

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

Labels (1)
1 Solution
734 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andy

yes it is supported on all ports. For usage it is necessary to follow i.MX6Q Sabre AI

SCH-27142_c.pdf p.6 design solution "SDa (SD3) power source for MX6 I/O."

SABRE|Automotive-Infotainment|i.MX6 | NXP 

For software use imx6q-sabreauto.dts and documentation on

i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

3 Replies
735 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andy

yes it is supported on all ports. For usage it is necessary to follow i.MX6Q Sabre AI

SCH-27142_c.pdf p.6 design solution "SDa (SD3) power source for MX6 I/O."

SABRE|Automotive-Infotainment|i.MX6 | NXP 

For software use imx6q-sabreauto.dts and documentation on

i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

734 Views
andychien
Contributor III

Dear Sir,

Thanks very much for your confirm.

We checked SCH-27142_c.pdf p.6 design solution "SDa (SD3) power source for MX6 I/O.".

The NVCC_SD3 is 3.3V.

Could you help check the support SDIO=208MHz is NVCC_SD =3.3V or 1.8V?

Thanks,

0 Kudos
734 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andy

please check sect.4.12.4.4 Bus Operation Condition for 3.3 V and 1.8 V Signaling

i.MX 6Dual/6Quad Applications Processors for Consumer Products - Data Sheet

Best regards
igor

0 Kudos