Hello,
One question about mcu bootloader on MCU Xpresso V11.01 and KinetisFlashTools.
Like i can see in the picture below it is possible to the mcu boot loader to launch an application whihout checking the crc.
I verify the code in mcu boot loader and it is true that it is possible to launch an application that the crc is not checking !
This seem to me a breach of security, because i can thrown anything ! even if the tag "kcfg" is necessary to disable the crc check.
My main question is that i don't understand the utility of disable crc check ?
Thanks by advance and Best regards from France
Didier JEANJEAN
Hi Didier,
MCUBoot doesn't check crc when downloading. It will check crc before jumping into application. You can see its call stack
get_active_peripheral() -> is_application_ready_for_executing() -> is_application_crc_check_pass()
If crc check fail, bootloader won't jump into application.
BTW, please make sure that BL_FEATURE_CRC_CHECK is defined as 1.
Regards,
Jing