LPC55S69 ISP下载

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S69 ISP下载

1,726 Views
haifeng_jin
Contributor III

hi  我在用NXP的LPC55S69的时候需要通过USB下载,但是在demo板上发现下载完了,没什么反应,应该是没有成功,工程是通过keil编译出来的gpio例程

pastedImage_1.png

Labels (1)
4 Replies

1,486 Views
mark2
Contributor III

Please use *.bin file with write-memory command.

If you want to use *.hex file, then use flash-image command.

0 Kudos

1,486 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello,

My name is Sabina and I would be more than happy to assist you. Could you please write you question in english to better understand what you need?

Thank you in advance!

Sabina

1,486 Views
haifeng_jin
Contributor III

Download via USB ISP, use blhost tool, but failed

0 Kudos

1,486 Views
Sabina_Bruce
NXP Employee
NXP Employee

Are you using USB 0 or USB1 for ISP mode?

BR,

Sabina

0 Kudos