AnsweredAssumed Answered

FRDM-KW36: How do I get an interrupt for each received BLE packet?

Question asked by Paul Matthis de mol on Oct 11, 2019
Latest reply on Oct 14, 2019 by Xiang Li

I am using a FRDM-KW36 and have modified the "hid_host bm" example for a BLE application. I need a counter for all received packets from all connected servers and must be able to associate them with each server.

 

I tried to use the Radio_1_IRQn interrupt for this, but I don't get as many interrupts as I would expect and can't distinguish the events.

I've also tried to get callbacks from the Bluetooth stack using the Controller_RegisterEnhancedEventCallback and Controller_ConfigureEnhancedNotification functions, but that doesn't seem to work and I'm not sure if the functions are intended for that at all.

 

Are there other ways to implement the counter that I overlooked?

 

Is there any form of documentation of the Blootooth stack that comes with the MCUXpresso SDK? I'm only guessing by the function names at the moment and that's very frustrating.

Outcomes