AnsweredAssumed Answered

Need MRFE6VS25 S-parameters that cover 30 to 100 MHz

Question asked by Eric Hooker on Oct 9, 2019

Does anyone have an S-Parameter file available for the MRFE6VS25GNR1 or MRFE6VS25NR1 that covers 30 MHz to 100 MHz?  The S-Parameter file on the NXP web site starts up at 200 MHz.  I would like to do some preliminary analysis from 30 to 100 MHz using S-parameters but they aren't available.  Also, I can't use the ADS model at this time since I don't presently have ADS.  I attached the .s2p file that is available on the NXP site but it's not sufficient for my needs.  Thank you. 

Attachments

Outcomes