AnsweredAssumed Answered

I.MX 6 DualLite 和 I.MX 6Q SABRE-SD的区别(difference between I.MX 6 DualLite and I.MX 6Q SABRE-SD)

Question asked by 铭恒 李 on Oct 7, 2019
Latest reply on Oct 8, 2019 by igorpadykov

我想请问这两个处理器之间的区别,目前的问题是 I.MX 6QSABRE-SD 的镜像是否合适 I.MX 6DualLite,在下载编译的时候是否需要在配置中的机器名将其区分 ( imx6qsabresd  和 imx6quallite)。因为原本我使用的imx6q 使用的Qt版本是5.6.2的,而新的imx6duallite 提供的则是5.3.0的。我使用的是4.1.15的内核。

 

I want to know the differences of image between  I.MX 6QSABRE-SD and I.MX 6DualLite. Cus the Qt version on I.MX 6DualLite is 5.3.0 but on I.MX 6QSABRE-SD is 5.6.2. I want to upgrate it so can I use the I.MX 6QSABRE-SD 's image into  I.MX 6DualLite ? Or I should set the machine name "imx6duallite" and compile again?

Outcomes