AnsweredAssumed Answered

imx8mm evk fails to boot with 4.9.123 image

Question asked by Samuel Woo on Oct 4, 2019
Latest reply on Mar 4, 2020 by Samuel Woo

Hi,

 

I am trying to boot 8MMINILPD4-EVK with NXP's demo image. The latest one (L4.14.98_2.0.0_ga_images_MX8MMEVK.zip) works fine, but with a previously released image (L4.9.123_2.3.0-ga_images_mx8mm.zip), the kernel keeps resetting itself without any error or kernel crash in the boot log. Rocko release of Yocto and Linux kernel 4.9 are particularly relevant to our project so booting with this image is critical. The same issue exists when booting from either SD card or eMMC. 

 

Has anyone had a similar issue or found a solution to this? The attached pdf contains the full boot log.

Attachments

Outcomes