Hi all,
I'm using MCUXpresso IDE with SDK 2.2. I'm currently looking over the example which is titled usb_device_cdc_vcom_bm . From what I understand, the code is a polling loop that reads user input one character once at a time and sends it to the program. My question is if there's a way to go backward and print out to the terminal from the program instead.
Thank you in advance!
Solved! Go to Solution.
Hi Sabina,
Thank you for the tip. That is in the right direction but it didn't work. However, I got it working now by following this example here. There's a couple more steps I have to do in addition to your suggestions.
https://community.nxp.com/thread/458760?commentID=939834#comment-939834
Thank you so much for your help!
Huy
Hello,
Can you please provide the part number of the mcu that you are using?
Also, just to make sure I understand, do you want to print on the terminal from the program as part of the execution, without needing to type or expect a user input?
Best Regards,
Sabina
Hi Sabina,
Thank you for the reply. I'm currently using the FRDM-KL25Z and yes you got it right, I just want to print on the usb terminal as part of the execution.
Best,
Huy
Hi Huy,
In this case if you'd like to use the same functions that are being used in the examples.
Take a look at how usb_echo() works.
usb_echo you will find that you can print directly in the console. For example,
usb_echo("Hello World!"\r\n);
and you will see hello world printed in the serial terminal that you are using.
If you see the root function it is essentially a printf.
Hope this helps. Let me know if I answered your question or if you have other questions.
Best Regards,
Sabina
Hi Sabina,
usb_echo would only print to the IDE's console. I want to print it to the usb terminal that is reading the user input instead.
For example, if I add a usb_echo line to line 640 and print out the character being received through the terminal like this
I will see this on the IDE's console.
and here's the terminal that I want to print to instead.
The hello world right here is written when I type it in. Now I want to be able to print something else instead of just what I typed in.
I hope that clarifies it.
Thanks,
Huy
Hello,
Ok in this case you can use the same function used in the example to send what you type.
USB_DeviceCdcAcmSend
However instead of sending an array that is being filled as you type, you can send an array that has a static string. Just make sure that you the size is corrected for your string.
Please try this and let me know your results. Try using a breakpoint to see if it writes as you expect.
Best Regards,
Sabina
Hi Sabina,
Thank you for the tip. That is in the right direction but it didn't work. However, I got it working now by following this example here. There's a couple more steps I have to do in addition to your suggestions.
https://community.nxp.com/thread/458760?commentID=939834#comment-939834
Thank you so much for your help!
Huy