On the iMX8M, does one need to terminate CLK1_P/N and CLK2_P/N when they are not used?
The Dev Kit schematic shows 100 Ohm parallel termination resistors, but there is no mention of how best to handle these un-used signals in the Hardware Development Guide.
Hello,
Customer may leave them floating if not used.
Hope this helps,
Best regards,
Aldo.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------