Hello community,
i have a problem using a SCL3711 with the NXP tagXplorer Software, maybe you can help me with it:
The TagXplorer detects my SCL3711 reader and it is possible to connect the reader. However pressing "connect" Tag does nothing, corresponding buttons remain grey.
(Pressing "connect Tag" / "disconnect tag" results in log-entry "Command APDU : FFFE00000160"
I tried NTAG216 and more tags from the "NFC Tag Starter Kit" with the same result.
Show Log:
2019.09.29.19.36.41 : Reader Name : SCM Microsystems SCL3711 reader & NFC device 0
2019.09.29.19.36.46 : Reader Connected Successfully : SUCCESS_OK
2019.09.29.19.36.49 : Command APDU : FFFE00000160
TagXplorer REV 1.2
Operating System Windows 10 Pro 1809 64bit
Java Version 8 update 221 (Build 1.8.0_221-b11)
SCM3711 reader Driver Version 1.13.0.0
Does anyone have a solution or suggestion?
Thank you
Harald
I found the reason for this problem: The SCL3711 is not supported...