What is the default radio power of the JN5169?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the default radio power of the JN5169?

Jump to solution
816 Views
qingshuzhuang
Contributor II

Hello everyone:

   I need help, this may be a simple question, but I am not finding the answer.

My environment:

   JN5169

   JN-AN-1219-Zigbee-3-0-Controller-and-Switch

Tags (2)
0 Kudos
1 Solution
682 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Qingshu Zhuang, I hope you're doing well!

 

By default, the provided examples use the highest available Tx power, however, this depends on which module version is being used, as, for example, the M05 and M06 modules are High Power.

 

Could you please confirm which module you're using? If you have a High Power module, you can follow the attached guide to enable high power mode.

 

Please let me know if you need more information.

 

Best regards,

Sebastian

View solution in original post

1 Reply
683 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Qingshu Zhuang, I hope you're doing well!

 

By default, the provided examples use the highest available Tx power, however, this depends on which module version is being used, as, for example, the M05 and M06 modules are High Power.

 

Could you please confirm which module you're using? If you have a High Power module, you can follow the attached guide to enable high power mode.

 

Please let me know if you need more information.

 

Best regards,

Sebastian