AnsweredAssumed Answered

about bitbake fsl-image-validation-imx -c populate_sdk

Question asked by y yq on Sep 24, 2019
Latest reply on Jan 23, 2020 by Yann Morvan

I get the following error when I create the SDK, the cmd line is :

DISTRO=fsl-imx-wayland MACHINE=imx8mqevk source fsl-setup-release.sh -b imx8m_build/

bitbake fsl-image-validation-imx

bitbake fsl-image-validation-imx -c populate_sdk

 

Transaction Summary
================================================================================
Install  1035 Packages

 

Total size: 555 M
Installed size: 3.3 G
Downloading Packages:
Running transaction check
Transaction check succeeded.
Running transaction test
Error: Transaction check error:
  file /etc/bluetooth/firmware.conf from install of linux-firmware-qca-1:0.0+git0+d114732723_a0026b646c+f6d0859f94-r0.noarch conflicts with file from package firmware-qca6174-2.0.3-r0.noarch

 

Error Summary
-------------

 


ERROR: fsl-image-validation-imx-1.0-r0 do_populate_sdk: Function failed: do_populate_sdk
ERROR: Logfile of failure stored in: /media/y/data/imx_yocto-bsp/imx8m_build/tmp/work/imx8mqevk-poky-linux/fsl-image-validation-imx/1.0-r0/temp/log.do_populate_sdk.22941
ERROR: Task (/media/y/data/imx_yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-fsl/images/fsl-image-validation-imx.bb:do_populate_sdk) failed with exit code '1'
NOTE: Tasks Summary: Attempted 6158 tasks of which 6157 didn't need to be rerun and 1 failed.

 

Summary: 1 task failed:
  /media/y/data/imx_yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-fsl/images/fsl-image-validation-imx.bb:do_populate_sdk
Summary: There was 1 WARNING message shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

Outcomes