AFM906N MET Model Parameters

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AFM906N MET Model Parameters

581 Views
tberezowsky
Contributor I

Hello Everyone, 

I'm not sure the best location to post this question. Please let me know! :smileyhappy:

I'd like use the AFM906N in a design around 140MHz, but NXP is not providing data below 240MHz. In addition, I do not have ADS or AWS, but if NXP or anyone else could provide me with the MET model parameters for the AFM906N so I can simulate in alternative SW, it would be greatly appreciated. 


Lastly, does anyone know why NXP will provide a reference DXF but not a schematic? 

Thanks! 

Tyler 

Tags (2)
0 Kudos
1 Reply

523 Views
tberezowsky
Contributor I

: ( Can I be given the S2P file at 140MHz? 

0 Kudos