Hello, I'd like to know if is possible to use MT29F8G08ABACAWP-IT with P1020/P1011?
If yes, how can I add support for that in u-boot and Linux kernel based on SDK 2.0.
Thanks
Leandro Schmitz
Hello, I'd like to know if is possible to use MT29F8G08ABACAWP-IT with P1020/P1011?
If yes, how can I add support for that in u-boot and Linux kernel based on SDK 2.0.
Thanks
Leandro Schmitz
I found the IS34ML04G081-TLI, it is a 4G bit memory; page size of 2048+64 with ECC of 1bit.
I appraciate if you could check if that is OK to use with P1020/P1011.
And how may I add support for that in u-boot and linux SDK 2.0
Thanks
Leandro
> is possible to use MT29F8G08ABACAWP-IT with P1020/P1011?
This is not possible.
The eLBC NAND controller of the P1020/11 is compatible with small (512 + 16 bytes) and large (2048 + 64 bytes) page parallel NAND Flash EEPROMs, while the MT29F8G08ABACAWP-IT has (4096 + 224 bytes) page.