Issue with MCUXpresso v11.0.1 and LPC55S69

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue with MCUXpresso v11.0.1 and LPC55S69

499 Views
cmkessell
Contributor I

I've been having difficulties using the MCUXpresso v11.0.1 debugger with a LPC55S69 evaluation kit (which has a revision 0A processor).  It worked fine with v11.0.0.

I notice that the v11.0.1 release notes mention that "Updates to allow LinkServer debug connections ... mean that some pre-production LPC55S6x silicon can no longer be supported."

Does my revision 0A processor count as "pre-production LPC55S6x silicon"?  If so is there any workaround to allow me to use the v11.0.1 IDE/debugger with my old processor?

0 Kudos
1 Reply

440 Views
soledad
NXP Employee
NXP Employee

Hi, 

MCUXpresso v11.0.1 doesn´t support pre-production LPC55S6x silicon as you mention, unfortunately, there is no a workaround, for an old processor you need to use MCUXpresso v11.0.0. 

 

Have a nice day!

Regards 

Soledad

0 Kudos