Hi,
I want to program flash for the addr(0x01100000),so I changed the demo “flash_program_erase_mpc5748g”as fllow:
#define BLOCK_START_ADDRS 0x01100000
#define BLOCK_END_ADDRS 0x01107FFF
.........
blockSelect.lowBlockSelect = 0x0U;
blockSelect.midBlockSelect = 0x0U;
blockSelect.highBlockSelect = 0x0U;
blockSelect.first256KBlockSelect = 0x10U;
blockSelect.second256KBlockSelect = 0x0U;
but the program failed to run and reported an error:
IVOR1_Handler() at core0_intc_sw_handlers.S:108 0x1002dae
so is there anything else that needs attention?
Hi,
where is your code running from? Notice that Read-While-Write is supported only between partitions. Flash block at 0x01100000 is located in partition 6, so the code must be executed from another partition or from RAM. Partition 6 is not accessible during program or erase operation.
Regards,
Lukas
Thank you very much for your help.