AnsweredAssumed Answered

bridge-utils problem

Question asked by sergio d'orazio on Sep 17, 2019
Latest reply on Sep 25, 2019 by karan gajjar

Hi ,

I am working with IMX6ULL EVK. I have compiled my yocto image adding in local.conf :

CORE_IMAGE_EXTRA_INSTALL += "bridge-utils"

 

On the EVK, when I put this command it work, the bridge-utils seams present:

 

root@imx6ull14x14evk:~# brctl
Usage: brctl [commands]
commands:
        addbr           <bridge>                add bridge
        delbr           <bridge>                delete bridge
        addif           <bridge> <device>       add interface to bridge
        delif           <bridge> <device>       delete interface from bridge
        hairpin         <bridge> <port> {on|off}        turn hairpin on/off
        setageing       <bridge> <time>         set ageing time
        setbridgeprio   <bridge> <prio>         set bridge priority
        setfd           <bridge> <time>         set bridge forward delay
        sethello        <bridge> <time>         set hello time
        setmaxage       <bridge> <time>         set max message age
        setpathcost     <bridge> <port> <cost>  set path cost
        setportprio     <bridge> <port> <prio>  set port priority
        show            [ <bridge> ]            show a list of bridges
        showmacs        <bridge>                show a list of mac addrs
        showstp         <bridge>                show bridge stp info
        stp             <bridge> {on|off}       turn stp on/off

 

 

On the EVK, when I put this command it not work, the bridge-utils seams not present :

 

root@imx6ull14x14evk:~# brctl addbr br0
add bridge failed: Package not installed
root@imx6ull14x14evk:~#

 

How can install bridge-utils ?

Can someone help me ?

 

Regards

Sergio D'Orazio.

Outcomes