AnsweredAssumed Answered

How to change RAM size in imx6slevk

Question asked by Sujay S on Sep 16, 2019
Latest reply on Sep 17, 2019 by Rita Wang

We use 1Gb RAM SOM with our imx6slevk 

I'm trying to change it to 512 MB

 

I ran ddr tester and got 

============================================
DDR Stress Test (3.0.0)
Build: Dec 14 2018, 14:12:40
NXP Semiconductors.
============================================

============================================
Chip ID
CHIP ID = i.MX6 SoloLite (0x60)
Internal Revision = TO1.2
============================================

============================================
Boot Configuration
SRC_SBMR1(0x020d8004) = 0x00002860
SRC_SBMR2(0x020d801c) = 0x01000001
============================================

ARM Clock set to 1GHz

============================================
DDR configuration
DDR type is DDR3
Data width: 32, bank num: 8
Row size: 14, col size: 10
Both chip select CSD0 and CSD1 are used
Density per chip select: 512MB
============================================

 

Where should I modify the source with these values?

Outcomes