Over voltage Power Supply effects on Kinetis K26 microcontroller IO's states

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Over voltage Power Supply effects on Kinetis K26 microcontroller IO's states

328 Views
puneeth_bheemar
Contributor I

Hello,

we are using Kinetis K26 microcontroller in our design. based on the datasheet, supply voltage is 3.3V +/- 10%. in normal operation supply voltage is well with in the mentioned range of 3.3V+/-10%.

However we would like to know the IO's state when power supply range goes above the maximum voltage of 3.6V (maximum of 4.1V).

will controller retain the previous state of IO's?

will the state of IO's will be tri-state / High impedance?

Thanks,

Puneeth KB

0 Kudos
1 Reply

266 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Puneeth,

No, it won't. Although supply power over 3.6v may harm to the device, it will not change the pin into tri-state or high-impedance.

Regards,

Jing

0 Kudos