imx-vpu-hantro updates for 4.14 kernel?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx-vpu-hantro updates for 4.14 kernel?

768 Views
jonathanolson
Contributor II

The imx-vpu-hantro depends on ION memory allocator APIs which became obsolete after kernel 4.12.

It seems that these kernel APIs were changed after 4.12 to use a dma buffers similar to the V4L2 APIs.

Are there any updates to imx-vpu-hantro to support the new kernel APIs?  I've checked up to the 1.13 release but no joy...

Better yet, I wish NXP would just replace imx-vpu-hantro with support for the V4L2 M2M hantro driver being developed for Rockchip which uses the same hantro codec.

0 Kudos
1 Reply

612 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Jonathan Olson,

My apologies for the delay.

There was a customer who successfully replaced the driver solution with the V4L2 implementation from Rockchip.

https://www.mail-archive.com/linux-media@vger.kernel.org/msg147671.html

There are plans for using V4L2 interface for controlling the Hantro VPU, but it will be based on the VeriSilicon driver and we don’t have a public roadmap as of today.

There are no plans for the moment to use DMABUF instead of ION in imx-vpu-hantro.

I hope this helps!

Regards,

0 Kudos