need for help,thank yoummc0:error -110 whilst initialising SD card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

need for help,thank yoummc0:error -110 whilst initialising SD card

1,217 Views
lvzhxiang
Contributor I

U-Boot 2015.04 (Feb 20 2017 - 11:18:01)

CPU: Freescale i.MX6UL rev1.1 at 396 MHz
CPU: Temperature 34 C
Reset cause: POR
Board: MX6UL 14x14 EVK
I2C: ready
DRAM: 512 MiB
force_idle_bus: sda=0 scl=0 sda.gp=0x1d scl.gp=0x1c
MMC: FSL_SDHC: 0, FSL_SDHC: 1
*** Warning - bad CRC, using default environment

Display: TFT70AB (800x480)
Video: 800x480x24
Error: no valid bmp image at 90000000 cfb_console.c
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc0 is current device
Net: FEC1
Error: FEC1 address not set.

Normal Boot
Hit any key to stop autoboot: 0
reading boot.scr
** Unable to read file boot.scr **
update firmware.........
reading /bin/zImage
6086336 bytes read in 281 ms (20.7 MiB/s)
reading /bin/ramdisk.img.u
8114750 bytes read in 367 ms (21.1 MiB/s)
reading /bin/imx6ul-14x14-evk.dtb
36258 bytes read in 23 ms (1.5 MiB/s)
Kernel image @ 0x80800000 [ 0x000000 - 0x5cdec0 ]
## Loading init Ramdisk from Legacy Image at 83800000 ...
Image Name:
Image Type: ARM Linux RAMDisk Image (gzip compressed)
Data Size: 8114686 Bytes = 7.7 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Using Device Tree in place at 83000000, end 8300bda1

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 3.14.38-6UL_ga (root@ubuntu) (gcc version 4.6.2 20110630 (prerelease) (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/10 09:20) ) #1 SMP PREEMPT Fri Mar 3 11:43:35 CST 2017
[ 0.000000] CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine model: Freescale i.MX6 UltraLite 14x14 EVK Board
[ 0.000000] cma: CMA: reserved 320 MiB at 8c000000
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] PERCPU: Embedded 8 pages/cpu @8bb3f000 s8320 r8192 d16256 u32768
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048
[ 0.000000] Kernel command line: console=ttymxc0,115200 cma=320M rdinit=/linuxrc
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 171964K/524288K available (7480K kernel code, 446K rwdata, 2648K rodata, 388K init, 432K bss, 352324K reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xa0800000 - 0xff000000 (1512 MB)
[ 0.000000] lowmem : 0x80000000 - 0xa0000000 ( 512 MB)
[ 0.000000] pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
[ 0.000000] modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
[ 0.000000] .text : 0x80008000 - 0x809ec4c0 (10130 kB)
[ 0.000000] .init : 0x809ed000 - 0x80a4e080 ( 389 kB)
[ 0.000000] .data : 0x80a50000 - 0x80abf8c0 ( 447 kB)
[ 0.000000] .bss : 0x80abf8cc - 0x80b2bbe4 ( 433 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] Switching to timer-based delay loop
[ 0.000019] sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655765682ns
[ 0.002693] clocksource_of_init: no matching clocksources found
[ 0.003070] Console: colour dummy device 80x30
[ 0.003119] Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
[ 0.003151] pid_max: default: 32768 minimum: 301
[ 0.003560] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.003588] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.005408] CPU: Testing write buffer coherency: ok
[ 0.005923] /cpus/cpu@0 missing clock-frequency property
[ 0.005963] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.006022] Setting up static identity map for 0x8071a718 - 0x8071a770
[ 0.040769] Brought up 1 CPUs
[ 0.040804] SMP: Total of 1 processors activated (6.00 BogoMIPS).
[ 0.040822] CPU: All CPU(s) started in SVC mode.
[ 0.041828] devtmpfs: initialized
[ 0.052654] VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5
[ 0.053456] pinctrl core: initialized pinctrl subsystem
[ 0.054399] regulator-dummy: no parameters
[ 0.077762] NET: Registered protocol family 16
[ 0.095613] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.097316] cpuidle: using governor ladder
[ 0.097344] cpuidle: using governor menu
[ 0.097652] Use WDOG1 as reset source
[ 0.116814] syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered
[ 0.117554] vdd3p0: 2625 <--> 3400 mV at 3000 mV
[ 0.118480] cpu: 725 <--> 1450 mV at 1150 mV
[ 0.119411] vddsoc: 725 <--> 1450 mV at 1175 mV
[ 0.125006] syscon 20e4000.iomuxc-gpr: regmap [mem 0x020e4000-0x020e7fff] registered
[ 0.132567] syscon 21ac000.romcp: regmap [mem 0x021ac000-0x021affff] registered
[ 0.134095] syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered
[ 0.141643] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.141675] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.145825] imx6ul-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
[ 0.148786] 20dc000.gpc supply pu not found, using dummy regulator
[ 0.180855] bio: create slab <bio-0> at 0
[ 0.187875] mxs-dma 1804000.dma-apbh: initialized
[ 0.188817] can-3v3: 3300 mV
[ 0.189418] VSD_3V3: 3300 mV
[ 0.190182] usb_otg1_vbus: 5000 mV
[ 0.191705] gpio_dvfs: 1300 <--> 1400 mV at 1400 mV
[ 0.193101] i2c-core: driver [max17135] using legacy suspend method
[ 0.193126] i2c-core: driver [max17135] using legacy resume method
[ 0.194498] SCSI subsystem initialized
[ 0.195782] usbcore: registered new interface driver usbfs
[ 0.195962] usbcore: registered new interface driver hub
[ 0.196291] usbcore: registered new device driver usb
[ 0.200392] i2c i2c-0: IMX I2C adapter registered
[ 0.202965] i2c i2c-1: IMX I2C adapter registered
[ 0.203267] Linux video capture interface: v2.00
[ 0.203456] pps_core: LinuxPPS API ver. 1 registered
[ 0.203476] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.203540] PTP clock support registered
[ 0.206375] MIPI CSI2 driver module loaded
[ 0.206966] Advanced Linux Sound Architecture Driver Initialized.
[ 0.209068] Bluetooth: Core ver 2.18
[ 0.209189] NET: Registered protocol family 31
[ 0.209209] Bluetooth: HCI device and connection manager initialized
[ 0.209252] Bluetooth: HCI socket layer initialized
[ 0.209284] Bluetooth: L2CAP socket layer initialized
[ 0.209371] Bluetooth: SCO socket layer initialized
[ 0.210358] cfg80211: Calling CRDA to update world regulatory domain
[ 0.211253] Switched to clocksource mxc_timer1
[ 0.237278] NET: Registered protocol family 2
[ 0.239291] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.239409] TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
[ 0.239566] TCP: Hash tables configured (established 4096 bind 4096)
[ 0.239682] TCP: reno registered
[ 0.239719] UDP hash table entries: 256 (order: 1, 8192 bytes)
[ 0.239777] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
[ 0.240374] NET: Registered protocol family 1
[ 0.241141] RPC: Registered named UNIX socket transport module.
[ 0.241173] RPC: Registered udp transport module.
[ 0.241193] RPC: Registered tcp transport module.
[ 0.241209] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.241987] Trying to unpack rootfs image as initramfs...
[ 1.735846] Freeing initrd memory: 7920K (83801000 - 83fbd000)
[ 1.738216] imx rpmsg driver is registered.
[ 1.739875] Bus freq driver module loaded
[ 1.742154] futex hash table entries: 256 (order: 2, 16384 bytes)
[ 1.760951] VFS: Disk quotas dquot_6.5.2
[ 1.761844] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 1.768009] NFS: Registering the id_resolver key type
[ 1.768131] Key type id_resolver registered
[ 1.768156] Key type id_legacy registered
[ 1.768254] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 1.770178] fuse init (API version 7.22)
[ 1.771476] msgmni has been set to 991
[ 1.780097] io scheduler noop registered
[ 1.780130] io scheduler deadline registered
[ 1.780637] io scheduler cfq registered (default)
[ 1.781854] imx-weim 21b8000.weim: Driver registered.
[ 1.787837] backlight.9 supply power not found, using dummy regulator
[ 1.791201] MIPI DSI driver module loaded
[ 1.796069] 21c8000.lcdif supply lcd not found, using dummy regulator
[ 1.801576] mxsfb 21c8000.lcdif: failed to find mxc display driver
[ 1.812029] Console: switching to colour frame buffer device 100x30
[ 1.818723] mxsfb 21c8000.lcdif: initialized
[ 1.826526] imx-sdma 20ec000.sdma: no event needs to be remapped
[ 1.826737] imx-sdma 20ec000.sdma: loaded firmware 3.1
[ 1.834827] imx-sdma 20ec000.sdma: initialized
[ 1.836272] Serial: IMX driver
[ 1.836891] 2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58, base_baud = 5000000) is a IMX
[ 2.585299] console [ttymxc0] enabled
[ 2.590647] 21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 59, base_baud = 5000000) is a IMX
[ 2.600550] 21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 60, base_baud = 5000000) is a IMX
[ 2.610263] serial: Freescale lpuart driver
[ 2.618425] imx sema4 driver is registered.
[ 2.622890] [drm] Initialized drm 1.1.0 20060810
[ 2.628631] [drm] Initialized vivante 1.0.0 20120216 on minor 0
[ 2.656296] brd: module loaded
[ 2.670963] loop: module loaded
[ 2.677595] spi_gpio spi4.15: gpio-miso property not found, switching to no-rx mode
[ 2.696432] CAN device driver interface
[ 2.703743] flexcan 2090000.can: device registered (reg_base=a0970000, irq=142)
[ 2.713849] flexcan 2094000.can: device registered (reg_base=a0978000, irq=143)
[ 2.723485] 20b4000.ethernet supply phy not found, using dummy regulator
[ 2.731561] pps pps0: new PPS source ptp0
[ 2.736122] fec 20b4000.ethernet (unregistered net_device): Invalid MAC address: 00:00:00:00:00:00
[ 2.745343] fec 20b4000.ethernet (unregistered net_device): Using random MAC address: 16:0e:61:f1:38:42
[ 2.755576] libphy: fec_enet_mii_bus: probed
[ 2.776290] fec 20b4000.ethernet eth0: registered PHC device 0
[ 2.783998] 2188000.ethernet supply phy not found, using dummy regulator
[ 2.792416] pps pps1: new PPS source ptp1
[ 2.796921] fec 2188000.ethernet (unregistered net_device): Invalid MAC address: 00:00:00:00:00:00
[ 2.806218] fec 2188000.ethernet (unregistered net_device): Using random MAC address: e6:e0:39:e5:ad:8a
[ 2.817697] fec 2188000.ethernet eth1: registered PHC device 1
[ 2.825323] PPP generic driver version 2.4.2
[ 2.830186] PPP BSD Compression module registered
[ 2.835014] PPP Deflate Compression module registered
[ 2.840286] usbcore: registered new interface driver cdc_ether
[ 2.846363] usbcore: registered new interface driver cdc_eem
[ 2.852357] usbcore: registered new interface driver cdc_ncm
[ 2.858053] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 2.864656] ehci-mxc: Freescale On-Chip EHCI Host driver
[ 2.870453] usbcore: registered new interface driver usb-storage
[ 2.876900] usbcore: registered new interface driver usbserial
[ 2.882949] usbcore: registered new interface driver usbserial_generic
[ 2.889616] usbserial: USB Serial support registered for generic
[ 2.895817] usbcore: registered new interface driver ftdi_sio
[ 2.901748] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 2.909192] usbcore: registered new interface driver option
[ 2.914955] usbserial: USB Serial support registered for GSM modem (1-port)
[ 2.922140] usbcore: registered new interface driver usb_ehset_test
[ 2.930689] 2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
[ 2.945596] 2184200.usb supply vbus not found, using dummy regulator
[ 2.955969] ci_hdrc ci_hdrc.1: EHCI Host Controller
[ 2.960950] ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
[ 2.981360] ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
[ 2.988832] hub 1-0:1.0: USB hub found
[ 2.992806] hub 1-0:1.0: 1 port detected
[ 2.998965] mousedev: PS/2 mouse device common for all mice
[ 3.006754] input: 20cc000.snvs-pwrkey as /devices/soc0/soc.0/2000000.aips-bus/20cc000.snvs-pwrkey/input/input0
[ 3.017643] snvs_pwrkey 20cc000.snvs-pwrkey: i.MX snvs powerkey probed
[ 3.024952] imx6ul-pinctrl 20e0000.iomuxc: pin MX6UL_PAD_RESERVE8 already requested by 20e0000.iomuxc; cannot claim for 0-0038
[ 3.036465] imx6ul-pinctrl 20e0000.iomuxc: pin-8 (0-0038) status -22
[ 3.042893] imx6ul-pinctrl 20e0000.iomuxc: could not request pin 8 (MX6UL_PAD_RESERVE8) from group edt_ft5x06grp on device 20e0000.iomuxc
[ 3.055477] edt_ft5x06 0-0038: Error applying setting, reverse things back
[ 3.062823] edt_ft5x06 0-0038: touchscreen probe failed
[ 3.068119] edt_ft5x06: probe of 0-0038 failed with error -5
[ 3.075922] input: iMX6UL TouchScreen Controller as /devices/virtual/input/input2
[ 3.085652] i2c-core: driver [isl29023] using legacy suspend method
[ 3.093314] i2c-core: driver [isl29023] using legacy resume method
[ 3.100739] rtc-rx8010 0-0032: Unable to write register #23
[ 3.106420] i2c i2c-0: probing for rx8010 failed
[ 3.111090] rtc-rx8010: probe of 0-0032 failed with error -5
[ 3.118204] snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0
[ 3.126904] i2c /dev entries driver
[ 3.131723] IR NEC protocol handler initialized
[ 3.136293] IR RC5(x) protocol handler initialized
[ 3.141103] IR RC6 protocol handler initialized
[ 3.145713] IR JVC protocol handler initialized
[ 3.150268] IR Sony protocol handler initialized
[ 3.154940] IR RC5 (streamzap) protocol handler initialized
[ 3.160536] IR SANYO protocol handler initialized
[ 3.165293] IR MCE Keyboard/mouse protocol handler initialized
[ 3.174055] pxp-v4l2 pxp_v4l2.10: initialized
[ 3.179663] i2c-core: driver [mag3110] using legacy suspend method
[ 3.185971] i2c-core: driver [mag3110] using legacy resume method
[ 3.193148] imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)
[ 3.201878] Bluetooth: HCI UART driver ver 2.2
[ 3.206359] Bluetooth: HCI H4 protocol initialized
[ 3.211172] Bluetooth: HCI BCSP protocol initialized
[ 3.216218] Bluetooth: HCIATH3K protocol initialized
[ 3.221489] usbcore: registered new interface driver bcm203x
[ 3.227348] usbcore: registered new interface driver btusb
[ 3.233107] usbcore: registered new interface driver ath3k
[ 3.239212] sdhci: Secure Digital Host Controller Interface driver
[ 3.245491] sdhci: Copyright(c) Pierre Ossman
[ 3.249875] sdhci-pltfm: SDHCI platform and OF driver helper
[ 3.258079] mmc0: no vqmmc regulator found
[ 3.301336] mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
[ 3.313006] mmc1: no vqmmc regulator found
[ 3.317156] mmc1: no vmmc regulator found
[ 3.371308] mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
[ 3.394139] fsl-quadspi 21e0000.qspi: unrecognized JEDEC id ffffff
[ 3.402510] mmc0: error -110 whilst initialising SD card
[ 3.409034] fsl-quadspi 21e0000.qspi: Freescale QuadSPI probe failed
[ 3.427605] usbcore: registered new interface driver usbhid
[ 3.433317] usbhid: USB HID core driver
[ 3.579957] mmc0: error -110 whilst initialising SD card
[ 3.751156] mmc0: error -110 whilst initialising SD card
[ 3.934728] mmc0: error -110 whilst initialising SD card
[ 4.026716] mmc1: BKOPS_EN bit is not set
[ 4.056706] mmc1: new high speed DDR MMC card at address 0001
[ 4.071231] mmcblk1: mmc1:0001 Q2J54A 3.64 GiB
[ 4.082365] mmcblk1boot0: mmc1:0001 Q2J54A partition 1 2.00 MiB
[ 4.094347] mmcblk1boot1: mmc1:0001 Q2J54A partition 2 2.00 MiB
[ 4.107360] mmcblk1rpmb: mmc1:0001 Q2J54A partition 3 512 KiB
[ 4.129283] mmcblk1: p1 p2 p3
[ 4.151496] mmcblk1boot1: unknown partition table
[ 4.162969] mmcblk1boot0: unknown partition table
[ 5.481278] wm8960 1-001a: Failed to issue reset
[ 5.486166] wm8960: probe of 1-001a failed with error -110
[ 5.494152] fsl-asrc 2034000.asrc: driver registered
[ 5.506949] imx-wm8960 sound.14: failed to find codec platform device
[ 5.513634] imx-wm8960: probe of sound.14 failed with error -22
[ 5.523172] NET: Registered protocol family 26
[ 5.527963] TCP: cubic registered
[ 5.532858] NET: Registered protocol family 10
[ 5.540121] sit: IPv6 over IPv4 tunneling driver
[ 5.546807] NET: Registered protocol family 17
[ 5.551418] can: controller area network core (rev 20120528 abi 9)
[ 5.557800] NET: Registered protocol family 29
[ 5.562383] can: raw protocol (rev 20120528)
[ 5.566683] can: broadcast manager protocol (rev 20120528 t)
[ 5.572433] can: netlink gateway (rev 20130117) max_hops=1
[ 5.578664] Bluetooth: RFCOMM TTY layer initialized
[ 5.583796] Bluetooth: RFCOMM socket layer initialized
[ 5.589011] Bluetooth: RFCOMM ver 1.11
[ 5.592863] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 5.598206] Bluetooth: BNEP filters: protocol multicast
[ 5.603612] Bluetooth: BNEP socket layer initialized
[ 5.608607] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 5.614618] Bluetooth: HIDP socket layer initialized
[ 5.619721] 8021q: 802.1Q VLAN Support v1.8
[ 5.624123] Key type dns_resolver registered
[ 5.629878] cpu cpu0: dev_pm_opp_get_opp_count: device OPP not found (-19)
[ 5.655201] gpio_dvfs: disabling
[ 5.658479] usb_otg1_vbus: disabling
[ 5.662194] VSD_3V3: disabling
[ 5.665277] can-3v3: disabling
[ 5.668355] regulator-dummy: disabling
[ 5.673192] imx mcc test is registered.
[ 5.677798] snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:02 UTC (2)
[ 5.705280] ALSA device list:
[ 5.708291] No soundcards found.
[ 5.713047] Freeing unused kernel memory: 388K (809ed000 - 80a4e000)
1+0 records in
1+0 records out
1024 bytes (1.0 kB) copied, 0.303101 s, 3.4 kB/s
sfdisk: Checking that no-one is using th[ 6.109122] mmcblk1: unknown partition table
is disk right now ...
sfdisk: OK

Disk /dev/mmcblk1: 119296 cylinders, 4 heads, 16 s[ 6.120064] mmcblk1: p1 p2 p3
ectors/track
sfdisk: /dev/mmcblk1: unrecognized partition table type
Old situation:
sfdisk: No partitions found
New situation:
Units: 1MiB = 1024*1024 bytes, blocks of 1024 bytes, counting from 0

Device Boot Start End MiB #blocks Id System
/dev/mmcblk1p1 10 509 500 512000 c W95 FAT32 (LBA)
/dev/mmcblk1p2 512 767 256 262144 83 Linux
/dev/mmcblk1p3 768 3727 2960 3031040 83 Linux
/dev/mmcblk1p4 0 - 0 0 0 Empty
sfdisk: Warning: no primary partition is marked bootable (active)
This does not matter for LILO, but the DOS MBR will not boot this disk.
Successfully wrote the new partition table

Re-reading the partition table ...

sfdisk: If you created or changed a DOS partition, /dev/foo7, say, then use dd(1)
to zero the first 512 bytes: dd if=/dev/zero of=/dev/foo7 bs=512 count=1
(See fdisk(8).)
129+0 records in
129+0 records out
132096 bytes (132 kB) copied, 0.037345 s, 3.5 MB/s
mount: special device /dev/mmcblk0p1 does not exist
dd: failed to open '/run/mmc0/system/u-boot.imx': No such file or directory
mkfs.vfat 2.11 (12 Mar 2005)
cp: cannot stat '/run/mmc0/system/boot.scr': No such file or directory
cp: cannot stat '/run/mmc0/system/zImage': No such file or directory
cp: cannot stat '/run/mmc0/system/ramdisk.img': No such file or directory
cp: cannot stat '/run/mmc0/system/imx6ul-14x14-evk.dtb': No such file or directory
cp: cannot stat '/run/mmc0/system/apps.tar.bz2': No such file or directory
cp: cannot stat '/run/mmc0/system/data.tar.bz2': No such file or directory
mke2fs 1.42.9 (28-Dec-2013)
[ 6.464888] random: mkfs.ext3 urandom read with 59 bits of entropy available
Filesystem label=
OS type: Linux
Block size=1024 (log=0)
Fragment size=1024 (log=0)
Stride=0 blocks, Stripe width=0 blocks
65536 inodes, 262144 blocks
13107 blocks (5.00%) reserved for the super user
First data block=1
Maximum filesystem blocks=67371008
32 block groups
8192 blocks per group, 8192 fragments per group
2048 inodes per group
Superblock backups stored on blocks:
8193, 24577, 40961, 57345, 73729, 204801, 221185

Allocating group tables: done
Writing inode tables: done
Creating journal (8192 blocks): done
Writing superblocks and filesystem accounting information: done

[ 8.463604] kjournald starting. Commit interval 5 seconds
[ 8.469307] EXT3-fs (mmcblk1p2): using internal journal
[ 8.474868] EXT3-fs (mmcblk1p2): mounted filesystem with ordered data mode
tar: can't open '/run/mmc0/system/apps.tar.bz2': No such file or directory
mke2fs 1.42.9 (28-Dec-2013)
Filesystem label=
OS type: Linux
Block size=4096 (log=2)
Fragment size=4096 (log=2)
Stride=0 blocks, Stripe width=0 blocks
189696 inodes, 757760 blocks
37888 blocks (5.00%) reserved for the super user
First data block=0
Maximum filesystem blocks=775946240
24 block groups
32768 blocks per group, 32768 fragments per group
7904 inodes per group
Superblock backups stored on blocks:
32768, 98304, 163840, 229376, 294912

Allocating group tables: done
Writing inode tables: done
Creating journal (16384 blocks): done
Writing superblocks and filesystem accounting information: [ 12.658205] random: nonblocking pool is initialized
done

[ 19.532607] kjournald starting. Commit interval 5 seconds
[ 19.538311] EXT3-fs (mmcblk1p3): using internal journal
[ 19.544344] EXT3-fs (mmcblk1p3): mounted filesystem with ordered data mode
tar: can't open '/run/mmc0/system/data.tar.bz2': No such file or directory
umount: /run/mmc0: not mounted
Update Complete!!!!!!!

0 Kudos
1 Reply

1,043 Views
igorpadykov
NXP Employee
NXP Employee

Hi Iv

for mmc0 errors one can check usdhc1 dts settings in

linux/arch/arm/boot/dts/imx6ul-14x14-evk.dts

imx6ul-14x14-evk.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

also recommended migrate to new kernels

linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos